The following list describes return loss (S11).
- Measures reflected power due to impedance mismatches in the
transmission path.
- Expressed in decibels (dB).
Equation 2.
- Higher absolute values indicate better impedance matching and
lower reflected power.
Note: The primary focus in this application note is maximizing trace impedance to enhance
return loss (S11) performance. Insertion loss (S21) can be minimized through trace length
reduction or adoption of low-loss dielectric materials. In contrast, S11 is more challenging
to manage as S11 requires stringent impedance control across the entire signal path.
Impedance control is the key of a successful design as this control not only directly
enhances S11, but also indirectly optimizes S21 by mitigating reflections and energy
dissipation.