Figure 3-1 shows the transmission line model used in the design example. The
impedance of a PCB transmission line is determined by the interplay
of trace width, trace thickness, substrate height, trace-to-copper
clearance, PCB dielectric constant (Dk), and coating above the
trace.
- Trace width: A wider trace increases the capacitive coupling
between the signal trace and the reference plane, which lowers the
impedance.
- Trace thickness: A thicker trace increases capacitive coupling
to the reference plane, this lowers the impedance slightly.
- Substrate height: A thinner dielectric layer (smaller distance
between the signal trace and reference plane) increases the
capacitive coupling, this lowers the impedance.
- Trace-to-copper clearance (ground strip separation): Narrower
clearance from the trace to adjacent copper increases fringe
capacitance coupling to neighboring copper. This reduces impedance
by increasing parasitic capacitance.
- PCB dielectric constant (Dk): A higher
dielectric constant increases the capacitance between the
trace and reference plane, thereby lowering the
impedance.
- Solder mask and solder coating: The
solder mask and solder coating adds a dielectric layer over
the signal trace. This increases the effective dielectric
constant (Dk) near the trace and lowers the impedance.
To main a consistent 50Ω transmission line impedance:
- Make sure of a uniform trace width and
spacing throughout the signal path.
- In PCB manufacturing, etched copper
traces have distortions and irregular rectangular
cross-sections due to the inherent etching factor. The
resulting profile is trapezoidal. In this design example,
the upper trace width is 5.3mil, while the lower width is
6.3mil. Align these geometric dimensions with the process
capability of the PCB fabricator.
Key recommendations for transmission line impedance:
- Use an impedance calculator to determine maximum impedance
parameters
- Close trace-to-copper spacing can reduce the impedance by 2Ω–3Ω,
consider the effects of the spacing
- Solder mask on the trace can reduce the impedance by 2Ω to 3Ω,
consider the effects of the solder mask
- Maintain impedance control of fabricated the PCB within 50Ω
±5%