SLAU367P October 2012 – April 2020 MSP430FR5041 , MSP430FR5043 , MSP430FR50431 , MSP430FR5847 , MSP430FR58471 , MSP430FR5848 , MSP430FR5849 , MSP430FR5857 , MSP430FR5858 , MSP430FR5859 , MSP430FR5867 , MSP430FR58671 , MSP430FR5868 , MSP430FR5869 , MSP430FR5870 , MSP430FR5872 , MSP430FR58721 , MSP430FR5887 , MSP430FR5888 , MSP430FR5889 , MSP430FR58891 , MSP430FR5922 , MSP430FR59221 , MSP430FR5947 , MSP430FR59471 , MSP430FR5948 , MSP430FR5949 , MSP430FR5957 , MSP430FR5958 , MSP430FR5959 , MSP430FR5962 , MSP430FR5964 , MSP430FR5967 , MSP430FR5968 , MSP430FR5969 , MSP430FR5969-SP , MSP430FR59691 , MSP430FR5970 , MSP430FR5972 , MSP430FR59721 , MSP430FR5986 , MSP430FR5987 , MSP430FR5988 , MSP430FR5989 , MSP430FR5989-EP , MSP430FR59891 , MSP430FR5992 , MSP430FR5994 , MSP430FR59941 , MSP430FR6005 , MSP430FR6007 , MSP430FR6035 , MSP430FR6037 , MSP430FR60371 , MSP430FR6041 , MSP430FR6043 , MSP430FR60431 , MSP430FR6045 , MSP430FR6047 , MSP430FR60471 , MSP430FR6820 , MSP430FR6822 , MSP430FR68221 , MSP430FR6870 , MSP430FR6872 , MSP430FR68721 , MSP430FR6877 , MSP430FR6879 , MSP430FR68791 , MSP430FR6887 , MSP430FR6888 , MSP430FR6889 , MSP430FR68891 , MSP430FR6920 , MSP430FR6922 , MSP430FR69221 , MSP430FR6927 , MSP430FR69271 , MSP430FR6928 , MSP430FR6970 , MSP430FR6972 , MSP430FR69721 , MSP430FR6977 , MSP430FR6979 , MSP430FR69791 , MSP430FR6987 , MSP430FR6988 , MSP430FR6989 , MSP430FR69891
Figure 19-4 shows the interface signals between the PSQ and the ASQ (see Section 21 for details).
Figure 19-4 USS Power Control NOTE
The control signals in Table 19-4 are internal only, and cannot be read or written by user software.
| Control Signal | Description | Condition to be Triggered |
|---|---|---|
| USS_PWRREQ | PSQ to power up the USS module and generate PSQ_START to the ASQ if UUPSCTL.ASQEN = 1 | Trigger one of the sources selected by UUPSCTL.USSPWRUPSEL |
| PSQ_START | ASQ to start a new measurement process if SAPHASCTL0.TRIGSEL = 1 | UUPSCTL.UPSTATE = 0 → 2 → 3 and UUPSCTL.ASQEN = 1 |
| PSQ_STOP | ASQ to stop the current measurement process | UUPSCTL.USSSTOP = 0 → 1 |
| ASQ_ACQDONE | Acknowledge PSQ that ASQ has completed the measurements | The measurements have been completed |
| ASQ_STDBYREQ | PSQ to enter STANDBY state | The measurements have been completed and SAPHASCTL1.ESOFF = 1 and SAPHASCTL1.STDBY = 1 |
| ASQ_PDREQ | PSQ to power off the USS module | The measurements have been completed and SAPHASCTL1.ESOFF = 1 and SAPHASCTL1.STDBY = 0 |