SLOSE88A December 2024 – March 2025 TAS6754-Q1
PRODUCTION DATA
For time-sensitive audio signals that require a minimal processing delay, such as active noise cancellation (ANC) or road noise cancellation (RNC), TAS6754-Q1 offers a low latency signal path. At 48kHz sampling frequency, this path reduces the signal delay by more than 70% between the input and output of the amplifier by minimizing the internal signal processing.
The low latency signal path is established in parallel to the regular audio signal path. When both signal paths are provided with input data, the two signals - audio and low latency - for each channel are internally mixed together right before the output amplification stage of the channel. Both signals are added together and the combined signal amplitude must not exceed the available gain range nor the voltage headroom to avoid distortion. Note that the low latency signals pass through the device with less delay than the regular audio path signals.
The low latency signal path is only available at a sampling frequency of 48kHz or 96kHz.