SLUSFN0A April 2025 – December 2025 BQ25630
PRODUCTION DATA
In ship mode, the BATFET is turned off to prevent the battery from powering the system. The host can place BQ25630 into ship mode by setting BATFET_CTRL = 10b. Ship mode has slightly higher quiescent current than shutdown mode, but QON can be used to exit from ship mode. The device is taken out of ship mode by either of these methods:
When the charger enters ship mode, the registers are reset to the POR values.
Ship mode is only entered when the adapter is not present. Setting BATFET_CTRL = 10b while VVBUS > VVBUS_UVLOZ (adapter present) either disables the BATFET or have no immediate effect depending on the setting of BATFET_CTRL_WVBUS.