SLUSFN0A April 2025 – December 2025 BQ25630
PRODUCTION DATA
The BATFET functions as a load switch between battery and system when the converter is not running. By changing the state of BATFET from on to off, systems connected to SYS can be power cycled. A system reset also resets all registers to POR state. Any of the following conditions initiate a system power reset:
When BATFET_CTRL_WVBUS is set to 1, system power reset proceeds if either SYS_RESET = 1b or QON is pulled low for tQON_RST, regardless of whether or not VBUS is present. There is a delay of tBATFET_DLY before initiating the system power reset. If QON is pulled low, there is no delay after the tQON_RST completes, regardless of BATFET_DLY setting. DIS_QON_RST bit can be set to 1b to disable system reset by QON press.
The system power reset can be initiated from the battery only condition, from OTG mode or from the forward charging mode with adapter present. If the system power is reset when the charger is in boost OTG mode, the boost OTG mode is first terminated by setting EN_OTG = 0b.