SLUSFN0A April 2025 – December 2025 BQ25630
PRODUCTION DATA
Type-C Specification 2.3 defines several cables, plugs, and receptacles to be used to attach ports. All cables, receptacles, and plugs that do not require VCONN power are supported. The device does not support any USB feature which requires USB Power Delivery communications over CC lines, such as e-marking or alternate mode.
USB-C added the ability to advertise as a port that sinks power (SNK), a port that sources power (SRC), or a dual role port (DRP) that can advertise both functions. The CC_MODE register selects if the device is advertising as SNK-only, SRC-only, or DRP capable.
USB-C detection is run through the CC1/CC2 lines to detect USB-C sources (Default / Medium / High), USB sinks, and legacy adapters. When DIS_CC = 0b (POR default), the detection algorithm automatically runs at all times. The orientation of the connected cable can be determined by reading the CC1_STAT and CC2_STAT registers when CC_ORIENT = 1.
After a connection is made, the USB-C detection routine can be forced to disconnect and restart by setting FORCE_CC_DET = 1b.