SLUSFN0A April 2025 – December 2025 BQ25630
PRODUCTION DATA
The device defaults to SNK-only mode. The device can be reconfigured to SNK-only mode through setting CC_MODE=00b.
In SNK mode, the device constantly presents pulldown resistors (Rd) on both CC pins to detect a 5V USB-C SRC device. The device continuously monitors the CC pins for the voltage level corresponding to the Type-C mode current advertisement by the connected SRC. As a SNK, the device detects and communicates the advertised current level of the connected SRC to the system through the VBUS_STAT register. The connected SRC can dynamically change the advertised current level after initial plug-in. When this occurs, IINDPM and VBUS_STAT is automatically updated accordingly.
If a SRC advertising default current is detected, it can be a USB-C to USB-C cable or a legacy USB-A to USB-C cable. BC 1.2 detection will be run automatically if EN_DPDM_DET = 1b in this case. If a legacy adapter is detected, IINDPM and VBUS_STAT will be set based on Section 8.3.4.2.