SLUSG21A May 2025 – September 2025 UCC25661
PRODUCTION DATA
When operation nears the inductive/capacitive boundary, the resonant current decreases before the gate is turned off. If the ISNS waveform is less than the VISNS_ZCS threshold, the gate pulse HO is terminated early instead of waiting for the VCR waveform to cross the VTH boundary. This early gate termination scheme is capable of leaving enough resonant current at the gate turn-off edge to drive the ZVS transition during the dead-time. Similar explanation holds good for the LO gate pulse.
The shape of the resonant current well below the resonant frequency poses some challenge for detecting the correct falling edge of the resonant current waveform. The UCC25661 implements additional logic to make sure that the correct falling edge of the ISNS signal is detected to avoid false tripping. To improve robustness against noise, the ISNS ZCS comparators are blanked at the rising edge of HO or LO gate. The same blanking time is used for both the VCR comparators and the ISNS ZCS comparators. When a ZCS event is detected, the internal soft start ramp voltage is slowly reduced. When the internal soft start ramps down, the switching frequency is also forced to increase, forcing the converter out of capacitive region. In the event of a persistent ZCS condition for a period of TZCSFault the UCC25661 controller ceases switching and move to the fault state.