SLVSHI9A March 2025 – September 2025 TPS7H5020-SEP , TPS7H5020-SP
PRODMIX
When utilizing peak current mode control in switching power converter design, the converter can enter into an unstable state when the duty cycle for the main power switch rises above 50%. Basically, the converter is in a state where the error between the peak current and average current increases with each subsequent switching cycle. This instability, known as subharmonic oscillation, can be mitigated by adding slope compensation. For the TPS7H502x, the slope compensation is in the form of a voltage ramp that is subtracted from the error amplifier output divided down by the parameter CCSR (COMP to CS_ILIM ratio). The minimum slope compensation for stability over the entire duty cycle range is equal to 0.5 × m, where m is the inductor falling current slope. The recommended slope compensation is 1 × m, as any increase above this value does not improve stability.
For the forward converter and boost converter, the slope compensation can be set equal to the downward slope of the output inductor current. For the flyback converter, the slope compensation is calculated using the downward slope of the current in the flyback transformer. In the isolated topologies, note that the sensed current waveform also needs to take into account the turns ratio of the transformer.
For forward:
For flyback:
For boost:
where:
For the TPS7H502x controller, a resistor from the RSC pin to AGND can be used to set the desired slope compensation. Equation 19 shows the calculation for determining the proper resistor value for RSC.
where: