SLVSHI9A March 2025 – September 2025 TPS7H5020-SEP , TPS7H5020-SP
PRODMIX
The turns ratio and primary inductance of the transformer are determined based on the target specifications of the converter. The turns ratio is calculated based on a maximum duty cycle of 35% targeted for the design.
A turns ratio of 2 is selected for the design. Based on the actual turns ratio, the minimum and maximum duty cycle can be calculated.
The primary inductance was calculated based on a 20% current ripple.
The primary inductance selected for the actual design was 30µH, which results in an actual ripple of approximately 25%. The following equations detail how to calculate transformer primary and secondary currents that are critical for proper design of the transformer. These equations are useful for defining the physical structure of the transformer.