SLVSHI9A March 2025 – September 2025 TPS7H5020-SEP , TPS7H5020-SP
PRODMIX
The CS_ILIM pin is driven by a signal representative of the main switch current of the power converter. The current signal has to have compatible input range of the COMP pin. As shown in Figure 7-9, the COMP pin voltage is used as the reference for the peak current. The output of the controller, OUT, is turned on by the internal clock signal and turned off when the peak of the sensed current signal reaches the COMP/CCSR pin voltage (which is approximately COMP/2). Note that this peak sensed current signal that is compared to COMP/CCSR at the PWM comparator contains an offset voltage of 150mV. The CS_ILIM pin is also used to configure the current limit for the controller. If slope compensation is implemented using the RSC pin, then the slope compensation ramp is subtracted from the COMP/CCSR signal, and turn-off of OUT occurs when the peak sensed current intersects the slope-compensated COMP/CCSR voltage. In instances which the user desires to bypass the internal error amplifier and drive COMP externally, the usable voltage range of the pin is approximately up to 2.3V. Since the CS_ILIM threshold for activating current limit is 1V and COMP is scaled down by CCSR, any external voltage applied to COMP that is greater than 2.3V is beyond the voltage to which the PWM comparator and feedback loop react.
A resistor from CS_ILIM to AGND is used to detect current for both proper PWM operation and overcurrent protection. The current limit threshold VCS_ILIM, is specified as 1V (nominal) in the electrical specifications. This indicates that when the voltage on this pin reaches this threshold, the device enters current limiting and turns off the output (OUT). Equation 15 shows the calculation for determining the value of the sense resistor for a selected current limit.
Note that the value of ILIM has to account for where and how the current is being sensed. In the case of an isolated converter using primary-side control with the sense resistor between source of primary FET to AGND, ILIM must be calculated appropriately with respect to the load current. Regardless of the topology, the user can make sure that there is sufficient margin between the peak current during normal operation and the overcurrent trip point when determining the value of RCS.