SLVSHI9A March 2025 – September 2025 TPS7H5020-SEP , TPS7H5020-SP
PRODMIX
The TPS7H502x output has a minimum on-time of approximately 135ns (typical). The minimum on-time is the smallest time duration for which the output remains in the on-state. As such, the minimum on-time can impose a restraint on the input-to-output conversion ratio of the power converter design. To overcome minimum on-time restrictions, careful selection of both the converter switching frequency and the transformer turns ratio (if applicable) is needed. For single switch forward, flyback, and boost converters in continuous conduction mode, the following equations can be used to check that the on time of the main power switch is sufficient for the intended design.
For forward:
where:
For flyback:
For boost:
Likewise, the minimum off-time also imposes restrictions on the converter operation. The minimum off-time is the smallest time duration that the output must remain off before subsequent turn-on. If the output is turned off during the switching cycle due to normal PWM operation, the output remains in the off-state for at least 40ns (typical). In most applications, the duty cycle of the converter during steady state remains well below 100% and allows for the output to be off much longer than this duration. The minimum off-time for the controller is not a concern for the TPS7H5021 in which the duty cycle is restricted to a 50% nominal maximum.
There are circumstances in which the minimum off-time must be taken into consideration when using the TPS7H5020 in power converter designs. Specifically, such cases occur when duty cycle is near 100% and turn-off happens close to the beginning of the next switching cycle. The intended off-time in these applications, as dictated by the converter feedback loop, is less than the minimum off-time of the controller. As such, the minimum off-time duration of the controller delays the output turn-on in the following switching cycle. While this must be taken into account at all operational frequencies, the effect is more pronounced at higher frequencies in which the minimum off-time constitutes a higher portion of the switching period. For example, at 1MHz switching frequency, the turn-on of the next cycle is delayed if the duty cycle surpasses 96% (nominal). To maintain the expected operation of the converter during steady-state, a maximum duty cycle can be imposed by the user on the converter design as shown in Equation 14.
where: