SLVSHX5A July 2025 – December 2025 TPS2HC08-Q1
PRODUCTION DATA
The device includes a temperature sensor on each power FET and within the controller portion of the device to monitor the temperature of each FET (TJ,FET) and the temperature of the controller (TJ,CONTROLLER). There are two cases that the device considers to be a thermal shutdown fault:
If either the above faults occur, the relevant switch is turned off. Each channel is turned off based on the measurement of the temperature sensor for that channel. As a result, if the thermal fault is detected on only one channel, the other channel continues normal operation.