SLVSHX5A July 2025 – December 2025 TPS2HC08-Q1
PRODUCTION DATA
To achieve good thermal performance, connect the VBB pad to a large copper pour. On the top PCB layer, the pour can extend beyond the package dimensions as shown in the layout examples below. In addition to this, having a VBB plane on one or more internal PCB layers and/or on the bottom layer is recommended. Vias must connect these planes to the top VBB pour. Connecting the VOUT1 and VOUT2 pads to large copper pours on the board can also help to achieve better thermal performance as the heat can transfer through the internal copper pillars to the large copper pours on the board.
TI recommends that the IO signals that connect to the microcontroller be routed to a via and then through an internal PCB layer.
If used in the design, the CIC capacitor, must be placed as close as possible to the VBB and GND pin of the device. If a ground network is used for reverse battery protection, the CIC capacitor must be connected from the VBB net to the IC_GND net. The CVBB capacitor must be placed close to the VBB pin and connected to system ground to allow for best performance.
The RLIM component must be placed close to the ILIM and GND pin of the device. If a ground network is used for reverse battery protection, the RLIM must be connected from the ILIM pin to the IC_GND net for expected current limit performance.
The FLT and SNS pin traces must be routed far apart (orthogonal or in different layers) to avoid any coupling between the two signals.
The TPS1HC03-Q1 device footprint is compatible with all other devices in the family and can be used for common board design.