If not already installed, then
install TICS Pro software from TI website: TICS Pro
Software
If the MATLAB® R2015b (9.0)* 64-bit runtime is not
already installed, download and install from MathWorks® website. While optional for
programming and evaluating the default profile settings, the MATLAB Runtime is
necessary for any application that needs to modify the DPLL loop filter
settings. See MATLAB Runtime.
Start TICS Pro software.
Select the LMK5B12212 profile from Select Device →
Network Synchronizer Clock (Digital PLLs) → LMK5B12212.
Confirm communications with the
board by:
Click USB
communications from the menu bar.
Click Interface to
launch the Communication Setup pop-up window.
Check these fields in the
Communication Setup pop-up window:
Make sure USB2ANY
is selected as the interface.
In case of
multiple USB2ANY, select desired interface. If a USB2ANY is
currently in use in another TICS Pro, then users must release
that interface by changing the interface setting to
DemoMode.
Click
Identify to blink LED shown in Figure 3-1. This confirms you are connected to the board you expect. Be
aware that USB2ANY devices connected to the PC but not attached
to by a TICS Pro instance can blink at a slow rate of 1 second
on, 1 second off continuously. After clicking the
Identify button, the LED flashes quickly at about 0.5
second on, 0.5 second off for about 5 seconds.