SPRACN0F October 2021 – March 2023 TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DK-Q1
Many common mathematical techniques in real-time control rely on the use of trigonometric functions: sine, cosine, and arc tangent are all examples. The TMU adds dedicated instructions to the C28x core for these functions as well as their inverse, that supersede the standard C library calls. As shown in #T5843526-55, significant cycle count reductions are possible using the TMU based instructions vs their Fast RTS counterparts.
There is also single instruction support for both square root as well as floating point division. These are often used in conjunction with the trigonometric functions previously listed. A full list of supported instructions and their cycle counts can be seen in Table 3-1. These instructions are inserted automatically by the C compiler on devices that have a TMU.
Operation | C Equivalent Operation | C28x Pipeline Cycles |
---|---|---|
Multiply by 2*pi | a = b * 2pi | 2 cycles + Sine/Cosine function |
Divide by 2*pi | a = b / 2pi | 2 cycles + Sine/Cosine function |
Divide | a = b / c | 5 cycles |
Square Root | a = sqrt(b) | 5 cycles |
Sin Per Unit | a = sin(b*2pi) | 4 cycles |
Cos Per Unit | a = cos(b*2pi) | 4 cycles |
Arc Tangent Per Unit | a = atan(b)/2pi | 4 cycles |
Arc Tangent 2 and Quadrant Operation | Operation to assist in calculating ATANPU2 | 5 cycles |