SPRACN0F October 2021 – March 2023 F29H850DM , F29H850TU , F29H859TU-Q1 , F29P329SM-Q1 , F29P589DM-Q1 , F29P589DU-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The memory blocks present in C2000 MCUs are parity or ECC protected. This helps in detecting memory corruptions if any. But parity/ECC feature can detect errors only if application does a read access to the memory. Hence it is very important to do a periodic readback of the memories to detect such issues earlier. Adding a CRC check for the memories confirms that the memory contents are unaltered.
The BGCRC module in C2000 MCUs can be used to perform readback of the memories in the background, hence ensuring uninterrupted execution of application without consuming any CPU cycles. Once triggered, it reads the memory contents in the background, computes CRC and compare it with the programmed golden value and flag error if there is mismatch. It also supports Scrub mode, where it does not perform a CRC comparison, but check for Parity/ECC errors. The reads happen during the idle time (when none of the other memory owners such as CPU, CLA, DMA are accessing the memory block) and hence the functional accesses are not impacted.
Figure 6-3 BGCRC Implementation on the
TMS320F2838xD Device