SPRACP8A March   2020  – May 2021 F28377D-SEP , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28076 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378D , TMS320F28378S , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384D-Q1 , TMS320F28384S , TMS320F28384S-Q1 , TMS320F28386D , TMS320F28386D-Q1 , TMS320F28386S , TMS320F28386S-Q1 , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   Trademarks
  2. 1Introduction
  3. 2Supplementary Online Information
  4. 3DCSM Security Tool Example Project
  5. 4DCSM Security Tool Configurable Options
    1. 4.1 ZONE1/ZONE2 Per LINKPOINTER Submodule
    2. 4.2 ZONE1/ZONE2 Header Submodule
  6. 5DCSM Security Tool Generated Content
  7. 6Adding DCSM Security Tool Support to an Existing Driverlib Project
  8. 7Summary
  9. 8References
  10. 9Revision History

ZONE1/ZONE2 Header Submodule

The first option inside each ZONEx Header module is selecting whether that zone's header is configured or left unchanged. In order to configure the ZONE, you must expand the ZONEx Header submodule and check the Configure this Section box.

ZONEx Header submodule can only be configured ONCE and ONCE ONLY. Once these options are configured, you CANNOT update them even by changing the LINKPOINTER. The ZONE1/ZONE2 Header submodule contain the following configurable options:

  • Password Lock: Disable/enable the Password Lock permanently. For more information, see the device-specific TRM.
  • CRC Lock: Disable/enable the CRC Lock permanently. For more information, see the device-specific TRM.
  • Configure Boot Section: This option determines whether to program the Boot Mode and Boot Pins.
For F2837xD, F2837xS and F2807x devices:
  • Boot Control PIN0/PIN1: These options select the boot pin0/pin1 for the device.
  • Get Mode: This is the boot mode for the device. The list of available options can be found in the device-specific TRM.
  • Boot Control Key and Boot Control Mode: These values are calculated based on the Get Mode option.
For F2838x, F28004x and F28002x devices:
  • Number of Boot Pins: This option will decide how many boot mode select pins (BMSP) are used, which in turn determines how many different boot modes can be defined.
  • Boot Mode Select Pins (BMSP0-2): These options select the boot pin0/pin1/pin2 for the device, if the BMSPx is within the usable range of Number of Boot Pins.
  • BOOTDEF0-7: These options select the boot mode for the device when the BMSP2-BMSP1-BMSP0 pin values match the BOOTDEF number. For example, in 3-pin boot select mode, BOOTDEF2 determines the boot mode for the device when BMSP2 pin is pulled LOW, BMSP1 pin is pulled HIGH and BMSP0 pin is pulled LOW.
For F28004x and F28002x devices:
  • ERRORSTS Pin: This options selects the ERRORSTS pin.
For F28002x and F2838x devices only:
  • Run MPOST: Selects the Memory Power on Self-Test mode.
For F2838x devices only:
  • Enable JTAGLOCK: Enables the JTAG lock protection on F2838x devices.
  • CMAC Key0 to Key4: The password keys for CMAC.
Note: For F28004x devices, boot mode configuration options are only available in ZONE1.
GUID-89DEC364-C85F-4004-BA70-19FE27B5D472-low.png Figure 4-4 ZONE1 Header Options
Note: The example ZONE1 Header Options shown are for F2837xD device.