SPRADN1 August   2025 F28E120SC , F29H850TU , F29H859TU-Q1 , TMS320F2800132 , TMS320F2800133 , TMS320F2800135 , TMS320F2800137 , TMS320F2800152-Q1 , TMS320F2800153-Q1 , TMS320F2800154-Q1 , TMS320F2800155 , TMS320F2800155-Q1 , TMS320F2800156-Q1 , TMS320F2800157 , TMS320F2800157-Q1 , TMS320F280021 , TMS320F280021-Q1 , TMS320F280023 , TMS320F280023-Q1 , TMS320F280023C , TMS320F280025 , TMS320F280025-Q1 , TMS320F280025C , TMS320F280025C-Q1 , TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1 , TMS320F280040-Q1 , TMS320F280040C-Q1 , TMS320F280041 , TMS320F280041-Q1 , TMS320F280041C , TMS320F280041C-Q1 , TMS320F280045 , TMS320F280048-Q1 , TMS320F280048C-Q1 , TMS320F280049 , TMS320F280049-Q1 , TMS320F280049C , TMS320F280049C-Q1 , TMS320F28075 , TMS320F28075-Q1 , TMS320F28374D , TMS320F28374S , TMS320F28375D , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376D , TMS320F28376S , TMS320F28377D , TMS320F28377D-EP , TMS320F28377D-Q1 , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28379D , TMS320F28379D-Q1 , TMS320F28379S , TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P550SG , TMS320F28P550SJ , TMS320F28P559SG-Q1 , TMS320F28P559SJ-Q1 , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction
  5. 2Features
    1. 2.1 Software Setup
    2. 2.2 Hardware Setup
  6. 3Running the C2000ware Example
  7. 4Adding Signal Sight to a Project
    1. 4.1 SysConfig Steps
    2. 4.2 Target Application Steps
    3. 4.3 CCS Steps
  8. 5Navigating the Signal Sight GUI
    1. 5.1 Verifying Target Connection
    2. 5.2 Enabling Data Streaming
    3. 5.3 Adjusting Plot View
    4. 5.4 Menu Bar Actions and Hotkeys
    5. 5.5 Advanced Features
      1. 5.5.1 Waveform Analyzer
      2. 5.5.2 Scope Settings
      3. 5.5.3 Data Export
  9. 6About the Tool
  10. 7Troubleshooting Guide
  11. 8Summary
  12. 9References

Running the C2000ware Example

A basic example called transfer_ex8_signalsight_basic_demo using the MCU Signal Sight tool is provided in the C2000ware SDK. Run this example to verify a valid hardware and software setup, as well as learn the features of the tool. Perform the following steps:

  1. Launch CCS
  2. Click File → Import Projects → Browse
  3. Navigate to the example in C2000WARE install path: C2000Ware_VERSION#/driverlib/DEVICE_GPN/examples/CORE_IF_MULTICORE/transfer/ folder.
  4. Click Finish
  5. Right-click on the project and click Properties
    1. Under General → Variables double-click on GUI_SUPPORT and change Value to 1
  6. Right-click on the project and click Debug Project
  7. Press Play in the Debug window
  8. Navigate to View → Plugins → myMCUSignalSight0
  9. Once the GUI loads, click Connect
  10. In the GUI window,
    1. Click Oscilloscope → Enable All Channels
    2. Set the Trigger Mode to manual
  11. View the sine, triangle, and square waveforms in the Signal

    Sight interface window

See Section 7 for debugging any issues which the user can experience when following these steps.