TIDUF75 April   2025

 

  1.   1
  2.   Description
  3.   Resources
  4.   Features
  5.   Applications
  6.   6
  7. 1System Description
    1. 1.1 Key System Specifications
  8. 2System Overview
    1. 2.1 System Block Diagram
    2. 2.2 Design Considerations
      1. 2.2.1  Determining the Number of eFuse Devices to use in Parallel
      2. 2.2.2  Setting up the Primary and Secondary Devices in a Parallel Configuration
      3. 2.2.3  Selecting the CDVDT Capacitor to Control the Output Slew Rate and Start-Up Time
      4. 2.2.4  Selecting the RIREF Resistor to set the Reference Voltage for Overcurrent Protection and Active Current Sharing
      5. 2.2.5  Selecting the RIMON Resistor to set the Overcurrent (Circuit Breaker) and Fast-Trip Thresholds During Steady-State
      6. 2.2.6  Selecting the RILIM Resistor to set the Current Limit and Fast-Trip Thresholds During Start-Up and the Active Sharing Threshold During Steady-State
      7. 2.2.7  Selecting the CITIMER Capacitor to Set the Overcurrent Blanking Timer
      8. 2.2.8  Selecting the Resistors to set the Under-voltage Lockout Threshold
      9. 2.2.9  Selecting the R-C Filter Between VIN and VDD
      10. 2.2.10 Selecting the Pullup Resistors and Power Supplies for SWEN, PG, FLT, and CMPOUT Pins
      11. 2.2.11 TVS Diode Selection at Input and Schottky Diode Selection at Output
      12. 2.2.12 Selecting CIN and COUT
    3. 2.3 Highlighted Products
      1. 2.3.1 TPS25985
      2. 2.3.2 LM94022 and LM94022-Q1
      3. 2.3.3 INA241x
      4. 2.3.4 TLV760
      5. 2.3.5 SN74LVC1G123
      6. 2.3.6 UCC27511A
      7. 2.3.7 CSD18510Q5B
  9. 3Hardware, Software, Testing Requirements, and Test Results
    1. 3.1 Hardware Requirements
    2. 3.2 Test Setup
    3. 3.3 Test Results
      1.      36
  10. 4Design and Documentation Support
    1. 4.1 Design Files
      1. 4.1.1 Schematics
      2. 4.1.2 Bill of Materials
      3. 4.1.3 Altium Project
      4. 4.1.4 Gerber Files
    2. 4.2 Tools
    3. 4.3 Documentation Support
    4. 4.4 Support Resources
    5. 4.5 Trademarks
  11. 5About the Author

Selecting the RILIM Resistor to set the Current Limit and Fast-Trip Thresholds During Start-Up and the Active Sharing Threshold During Steady-State

RILIM is used in setting up the active current sharing threshold during steady-state and the overcurrent limit during start-up among the devices in a parallel chain. Each device continuously monitors the current flowing through (IDEVICE) and outputs a proportional analog output current on the ILIM pin. This, in turn, produces a proportional voltage (VILIM) across the respective ILIM pin resistor (RILIM), which is expressed as Equation 11.

Equation 11. VILIM=IDEVICE×GILIM×RILIM

GILIM is the current monitor gain (IILIM : IDEVICE), with a typical value of 18.18μA/A.

  • Active current sharing during steady-state: This mechanism operates only after the device reaches steady-state and acts independently by comparing the load current information (VILIM) with the Active Current Sharing reference (CLREFLIN) threshold, defined as Equation 12.
    Equation 12. CLREFLIN=1.1×VIREF3
    Therefore, RILIM must be calculated using Equation 13 to define the active current sharing threshold as IOCP(TOTAL) / N, where N is the number of devices in parallel. Using N = 6, RIMON = 167Ω, and Equation 13, RILIM can be calculated to be 367.4Ω. The closest standard value of 365Ω with 0.1% tolerance and power rating of 100mW resistances are selected as RILIM for each device.
    Equation 13. RILIM=1.1×N×RIMON3
    Note:

    To determine the value of RILIM, Equation 14 must be used if a different threshold for active current sharing (ILIM(ACS)) than IOCP / N is desired.

    Equation 14. RILIM=1.1×VIREF3×GILIM×ILIM(ACS)

    When computing the current limit threshold during start-up in the next subsection, be sure to use this RILIM value.

  • overcurrent limit during start-up: During inrush, the overcurrent condition for each device is detected by comparing the load current information (VILIM) with a scaled reference voltage as depicted in Equation 15.
    Equation 15. C L R E F S A T = 0.7 × V I R E F 3
    The current limit threshold during start-up can be calculated using Equation 16.
    Equation 16. I I L I M S t a r t u p = C L R E F S A T G I L I M × R I L I M
    By using a RILIM value of 365Ω for each device, the start-up current is limited to about 35A for each device and the ILIM(ACS) is set at about 55A.
    Note: The active current limit block employs a fold-back mechanism during start-up based on VOUT. When VOUT is below the fold-back threshold (VFB) of 1.99V, the current limit threshold is further lowered.