TIDUF75 April 2025
When the device interrupts a large amount of current instantaneously causing a short circuit and overload current limit, the input inductance generates a positive voltage spike on the input, whereas the output inductance creates a negative voltage spike on the output. The peak amplitudes of these voltage spikes (transients) are dependent on the value of inductance in series with the input or output of the device. Such transients can exceed the absolute maximum ratings of the device and eventually lead to failures due to electrical over-stress (EOS) if appropriate steps are not taken to address this issue. Typical methods for addressing this issue include:
See also TVS Clamping in Hot-Swap Circuits and Selecting TVS Diodes in Hot-Swap and ORing Applications for details on selecting an appropriate TVS diode and the number of TVS diodes to be in parallel to effectively clamp the positive transients at the input below the absolute maximum ratings of the IN pin (20V). These TVS diodes also help to limit the transient voltage at the IN pin during the Hot Plug event. Five (5) 5.0SMDJ12A are used in parallel in the TIDA-050077.
Select Schottky diodes based on the following criteria:
Five (5) PMEG045V100EPE-QZ devices are used in parallel in the TIDA-050077.