TIDUF85A August 2024 – December 2024
If the arc gap is increase too much during arc testing, the arc extinguishes and the full string voltage is applied across the arc gap. This means the voltage is still above the threshold of the isolated comparator, but arcing is no longer present. The window comparator circuit can be also be used to catch these cases, to set a lower threshold for when arcing is starting and an upper threshold for when the arc is stopping.