TIDUF85A August 2024 – December 2024
Figure 3-8 shows the setup for testing with real arcs. An arc generator is needed to emulate real-world arcs. The string of PV panels can be emulated by a DC current source. In that case, a decoupling and line impedance network is necessary to imitate the impedance of the solar cabling. The exact setup and testing scenarios are described in the relevant norms like UL1699B.
For the arc labeling circuit, it is important to connect the voltage across the arc generator with low impedance to the arc labeling circuit input J9. The string current needs to be feed through the current transformer. Connect the string voltage to connector J8.
The description of the software tools and workflow on how to gather and label data, train an embedded AI model and validate the model is beyond the scope of this document. Links to detailed descriptions, user guides, tools and other resources are available in the product folder of TIDA-010955 and TIEVM-ARC-AFE. The required software is part of the C2000WARE-DIGITALPOWER-SDK.