TIDUF85A August 2024 – December 2024
AMC3330 used for both voltage sensing paths has a differential signal output. To interface this signal to the single-ended ADC of the C2000 MCU a conversion stage is implemented using TLV6001. See also the Interfacing a Differential-Output (Isolated) Amp to a Single-Ended Input ADC application brief. R92 is not populated, since the input voltage is always positive, which means no biasing is required. The gain of this conversion stage is set by the relation between R60 and R84 and R87 and R86. A gain of 1.65 is used, since the maximum output of AMC3330 is 2V and the maximum input of the ADC is 3.3V.