TIDUF85A August 2024 – December 2024
Figure 3-2 shows the transfer function of the current transformer circuit with different DC currents applied. This is done by feeding two cables through the current transformer. One is carrying a AC signal with varying frequency for the AC analysis, while the second cable is carrying a DC current. The input current is measured with a high-performance current probe of an oscilloscope. The output voltage is measured on TP9 which is labeled CT+.
High DC currents lead to saturation effects especially for low frequencies. In the band from 30kHz to 100kHz which is used for arc detection the attenuation is around 3dB for a current of 20A which is acceptable. If higher DC currents are present in the system, an external sensor which can handle these currents can be used. The signal chain needs to be adjusted accordingly.
Figure 3-3 shows the transfer curve between the output of the CT circuit and the output of the gain stage. A stable gain of 20dB (Gain of 10) is achieved up 100kHz which is the upper limit of the frequency range used for arc detection.
Figure 3-4 and Figure 3-5 show the transfer curves of the filter stage. Channel 1 and channel 2 are implemented as a 8th order band-pass filter while channel 3 and channel 4 are implemented as a 4th order band-pass filter. These transfer curves are measured between TP2 (output of the gain stage) and TP1 (output of the band-pass filter stage).
Figure 3-2 and Figure 3-3 show the transfer curves of the complete signal chain for channel 1 with a 8th order band-pass filter and channel 3 with a 4th order band-pass filter.