TIDUFF8 September 2025
To get absolute position, this reference design uses dual track coils with coprime periods. The outer side track uses 16 periods coils while the inner track uses 15 periods coils.
To better illustrate how to calculate the absolute position, the design guide takes the outer coil with four periods and the inner coil with three periods, for example.
Figure 3-8 illustrates the relationship between the electrical angle of the outer coils and inner coils over one mechanical revolution with a lower period count of four and three for simplicity.
The absolute mechanical angle is determined by the electrical angle difference between the coprime coils in the example 4 and 3.
| DIFFERENCE ANGLE (°) | ABSOLUTE ANGLE (°) |
|---|---|
| 0 to 90 | N4(1) |
| –270 to –240 | 90 + N4(1) |
| 120 to 180 | 90 + N4(1) |
| –180 to 120 | 180 + N4(1) |
| 240 to 270 | 180 + N4(1) |
| –90 to 0 | 270 + N4(1) |
In this reference design, coprime 16 and 15 coils are used. The 16 periods coils divide the absolute angle into 16 sectors. Assuming the absolute angle falls within nth sector, the outer coils angle are either n × 22.5° greater than or 360 – n × 22.5° less than the inner coils angle. Equation 3 calculates the sector number.
Then, the absolute angle can be calculated as:
Figure 3-9 shows the absolution position calculation flow chart in a Nonius encoder.