TIDUFF8 September 2025
Connect the encoder with a 12V supply, record the current consumption of the whole encoder.
The current consumption under 12V power supply is 39mA. This value includes both the consumption of the coil and the consumption of all signal chain chips. Resolver has similar working principles with inductive encoder which also needs to inject an excitation signal, but resolver typically needs higher excitation current from 40mA to 200mA. Inductive encoder has significant advantages on power consumption compared with resolver.