TIDUFG2 December 2025
Figure 4-3 shows the transfer function of the bandpass filter from section 3.1.3. An AC input from the signal generator is injected into the input of C6 separated from the integrator output trace. The output of the bandpass filter is measured with the high bandwidth passive probe of the oscilloscope at the output of R22.

Figure 4-4 shows the band-pass output noise. This noise is less than the resolution of a 12-bit, 3.3V ADC.
Figure 4-4 Output Noise of Band-Pass
FilterFigure 4-5 shows the output of the low-pass filter with a resistive load of 9.74A. The RMS voltage corresponds to Equation 4.
Figure 4-5 Low-Pass Filter Output With Resistive
LoadFigure 4-6 and Figure 4-7 show the LOG300 output for normal vs arcing for a two different loads. This demonstrates how the arcing signal reaches up to the 1MHz to 10MHz range but noise from the loads is significantly reduced. For Figure 4-6 and Figure 4-7, the top subplot shows the LOG300 output, the bottom subplot shows the oscilloscope current probe output.
Figure 4-6 Vacuum Motor Load – Top: LOG300 Bottom: Current Probe
Figure 4-7 600W Tungsten Lamp With Dimmer Load – Top: LOG300 Bottom: Current Probe