SBOU024C august 2004 – july 2023 PGA309
The Over-Scale and Under-Scale Limit circuit provides a programmable upper and lower clip limit for the PGA309 output voltage. This circuit can be enabled by setting Register 5, bit D6 to ‘1’. When combined with the Fault Monitor circuitry, system diagnostics can be performed to determine if a conditioned sensor is defective or if the process being monitored by the sensor is out of range. Figure 2-24 details the key sections of the Over-Scale and Under-Scale Limit circuit. The selected PGA309 VREF is divided down by a precision resistor string to form the over-scale and under-scale thresholds, as shown in Table 2-18 and Table 2-19. Register 5 bits [5:0] set the desired thresholds. These resistor ratios are extremely accurate and produce no significant initial or temperature errors. As shown in Figure 2-24, there are two separate comparators: over-scale and under-scale, which use the over-scale or under-scale threshold, respectively, and determine where the PGA309 output (VOUT) will be clipped. The dominant errors in the Over-Scale and Under-Scale Limit circuit are due to the comparators offset and offset temperature drift.
HL2 [5] |
HL1 [4] |
HL0 [3] |
Over-Scale Threshold (V) |
Over-Scale Threshold |
---|---|---|---|---|
0 | 0 | 0 | 4.854 | 0.9708 VREF |
0 | 0 | 1 | 4.805 | 0.9610 VREF |
0 | 1 | 0 | 4.698 | 0.9394 VREF |
0 | 1 | 1 | 4.580 | 0.9160 VREF |
1 | 0 | 0 | 4.551 | 0.9102 VREF |
1 | 0 | 1 | 3.662 | 0.7324 VREF |
1 | 1 | 0 | 2.764 | 0.5528 VREF |
1 | 1 | 1 | Reserved | — |
LL2 [2] |
LL1 [1] |
LL0 [0] |
Under-Scale Threshold (V) |
Under-Scale Threshold |
---|---|---|---|---|
0 | 0 | 0 | 0.127 | 0.02540 VREF |
0 | 0 | 1 | 0.147 | 0.02930 VREF |
0 | 1 | 0 | 0.176 | 0.03516 VREF |
0 | 1 | 1 | 0.196 | 0.03906 VREF |
1 | 0 | 0 | 0.225 | 0.04492 VREF |
1 | 0 | 1 | 0.254 | 0.05078 VREF |
1 | 1 | 0 | 0.274 | 0.05468 VREF |
1 | 1 | 1 | 0.303 | 0.06054 VREF |
The design considerations in using the Over-Scale and Under-Scale Limit circuit are best understood through a definition by example, as shown in Example2-4.