SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Similar requirement exist when the Sensor Controller and Timer01 uses events that have synchronous origin. If the operational rate of the event subscriber is lower than the operational rate of the event publisher, the subscriber may lose events. This happens when the event duration is shorter than the effective clock period of the subscriber module. The following consequences arise from this: