SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
For AES-CTR operations, the following configuration parameters are required:
The length field can have any value. If a data stream is finished and the next data stream uses the same key and control, only the IV and length field can be written with a new value. The length field can be 0, resulting in continued processing.
If the result IV must be read by the host, the save_context bit must be set to 1 after processing the programmed number of bytes.