SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
If pParams->initConfig.bDynamicWinOffset is 1, the radio CPU shall perform automatic calculation of the WinSize and WinOffset parameters in the transmitted CONNECT_IND or AUX_CONNECT_REQ message. WinSize is byte 7 of the payload, and WinOffset is byte 8 and 9 (see the Bluetooth Specification documents listed in Related Documentation). The radio CPU shall find the possible start times of the first connection event from the pParams->connectTime parameter and the connection interval, which shall be given in units of 1.25 ms by the Interval field (byte 10 and 11) from the payload to be transmitted (see the Bluetooth Specification documents listed in Related Documentation). The possible times of the first connection event are any whole multiple of connection intervals from pParams->connectTime, which may be in the past or the future from the start of the initiator command.
The radio CPU shall insert a WinOffset parameter in the transmitted CONNECT_IND or AUX_CONNECT_RSP such that the first connection event is signaled to be at the first connection event that comes sufficiently long after the end of the CONNECT_IND or AUX_CONNEXT_REQ packet to be transmitted. This means that the time from the end of the CONNECT_IND or AUX_CONNECT_REQ packet to the start of the first packet in the connection is between transmitWindowDelay + WinOffset and transmitWindowDelay + WinOffset + WinSize, where transmitWindowDelay is 1.25 ms when a CONNECT_IND PDU is used, 2.5 ms when an AUX_CONNECT_REQ PDU is used on an LE Uncoded PHY, and 3.75 ms when an AUX_CONNECT_REQ PDU is used on the LE Coded PHY, (for details, see the Specification of the Bluetooth System, Version 5.0 listed in Related Documentation). The radio CPU shall set up the transmit window (WinOffset and WinSize) so that there is margin both between the start of the transmit window and the start of the first master packet and between the start of the first master packet and the end of the transmit window (see the Specification of the Bluetooth System, Version 5.0 listed in Related Documentation). The inserted WinSize shall be either 1 or 2; ensuring such a margin. The margin is set to the correct value through an override in the BLE stack (see Section 26.8.4).
The radio CPU shall write the calculated values for WinSize and WinOffset into the corresponding locations in the pParams->pConnectData buffer. The start time of the first connection event to be used in order to transmit the first packet within the signaled transmit window shall be written back by the radio CPU in pParams->connectTime. If no connection is made, the radio CPU shall add a multiple of connection intervals to pParams->connectTime so that it is the first possible time of a connection event after the operation ended.