SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Command ID number: 0x0403
CMD_GET_RSSI is an immediate command that takes no parameters, and therefore, can be used as a direct command.
On reception, the radio CPU reads the RSSI from an underlying receiver. The RSSI is returned in result byte 2 (bit 23–16) of CMDSTA (see Figure 26-5). The RSSI is given on signed form in dBm. If no RSSI is available, this is signaled with a special value of the RSSI (−128, or 0x80).
If no radio operation command is running, the radio CPU returns the result ContextError in CMDSTA. Otherwise, the radio CPU returns DONE along with the RSSI value.