SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
During an SRAM write, a parity bit is calculated and stored for each byte that is written. Parity error detection is done on a byte-wide basis during an SRAM read operation. This means that a parity error on any byte in a memory read operation causes a memory data error to be detected. A parity error causes a processor bus fault exception (see Section 6.1.2).
The SRAM address that was read during parity error detection is captured in the SRAM_MMR:PER_CHK register. This parity error address is stored as an offset from the base address of SRAM memory.