To start:
- Install Code Composer Studio from the Code Composer Studio (CCS) Integrated Development Environment (IDE) tools folder. Version 12.0 or above is recommended.
- Install C2000WARE-DIGITAL-POWER-SDK in one of two ways:
- Through the C2000Ware Digital Power SDK tools folder
- Go to CCS and under View → Resource Explorer. Under the TI Resource Explorer, go to C2000WARE-DIGITAL-POWER-SDK, and click on the install button.
- When installation completes, close CCS, and open a new workspace. CCS automatically detects powerSUITE. A restart of CCS may be required for the change to be effective.
Note: powerSUITE is installed with the SDK by default.
The firmware project can now be imported as
follows:
The user can also directly import the project, by going inside CCS to Click Project → Import CCS Projects and browsing to the solution folder located at <SDK>/solutions/tidm_02013/f28003x/ccs.
A project spec will appear, clicking on this will create a self-contained folder of the project with all the dependencies inside it.