TIDUF18A October 2022 – February 2024
Due to the input double-line frequency ripple on the DC link capacitor, its capacitance is mainly determined by the output voltage ripple, as calculated in Equation 19:
where,
The actual capacitor used is 1410 µF(3 x 470uF).