Optionally, to verify active synchronous rectification, the user can also probe the PWM signals and see the change in duty cycle. To connect the probe for it, the user must first stop the power stage as outlined below and de-energize all circuits under test.
Once finished, reduce the input voltage, VPRIM, to zero. Watch for the voltages in the watch window to reduce down to zero.
Fully halting the MCU when in real-time mode is a two-step process. First,
halt the processor by using the Halt button on the toolbar , or by using Target →
Halt. Then, take the MCU out of real-time mode by clicking on . Finally, reset the MCU
.
Close the CCS debug session by clicking Terminate Debug Session
(Target → Terminate
all).