SPRUJ79 November 2024 F29H850TU , F29H859TU-Q1
Table 24-262 lists the memory-mapped registers for the ADC_GLOBAL_REGS registers. All register offset addresses not listed in Table 24-262 should be considered as reserved locations and the register contents should not be modified.
| Offset | Acronym | Register Name | Protection |
|---|---|---|---|
| 0h | ADCSOCFRCGB | ADC Global SOC Force | PARITY |
| 4h | ADCSOCFRCGBSEL | ADC Global SOC Force Select | PARITY |
| 8h | PARITY_TEST_ALT1 | Enables parity test |
Complex bit access types are encoded to fit into small table cells. Table 24-263 shows the codes that are used for access types in this section.
| Access Type | Code | Description |
|---|---|---|
| Read Type | ||
| R | R | Read |
| R-0 | R -0 | Read Returns 0s |
| Write Type | ||
| W | W | Write |
| W1S | W 1S | Write 1 to set |
| Reset or Default Value | ||
| -n | Value after reset or the default value | |
| Register Array Variables | ||
| i,j,k,l,m,n | When these variables are used in a register name, an offset, or an address, they refer to the value of a register array where the register is part of a group of repeating registers. The register groups form a hierarchical structure and the array is represented with a formula. | |
| y | When this variable is used in a register name, an offset, or an address it refers to the value of a register array. | |
ADCSOCFRCGB is shown in Figure 24-280 and described in Table 24-264.
Return to the Summary Table.
ADC Global SOC Force
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| SOC31 | SOC30 | SOC29 | SOC28 | SOC27 | SOC26 | SOC25 | SOC24 |
| R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h |
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| SOC23 | SOC22 | SOC21 | SOC20 | SOC19 | SOC18 | SOC17 | SOC16 |
| R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h |
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| SOC15 | SOC14 | SOC13 | SOC12 | SOC11 | SOC10 | SOC9 | SOC8 |
| R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h |
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| SOC7 | SOC6 | SOC5 | SOC4 | SOC3 | SOC2 | SOC1 | SOC0 |
| R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h | R-0/W1S-0h |
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31 | SOC31 | R-0/W1S | 0h | Indicate if SOC31 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 30 | SOC30 | R-0/W1S | 0h | Indicate if SOC30 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 29 | SOC29 | R-0/W1S | 0h | Indicate if SOC29 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 28 | SOC28 | R-0/W1S | 0h | Indicate if SOC28 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 27 | SOC27 | R-0/W1S | 0h | Indicate if SOC27 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 26 | SOC26 | R-0/W1S | 0h | Indicate if SOC26 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 25 | SOC25 | R-0/W1S | 0h | Indicate if SOC25 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 24 | SOC24 | R-0/W1S | 0h | Indicate if SOC24 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 23 | SOC23 | R-0/W1S | 0h | Indicate if SOC23 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 22 | SOC22 | R-0/W1S | 0h | Indicate if SOC22 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 21 | SOC21 | R-0/W1S | 0h | Indicate if SOC21 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 20 | SOC20 | R-0/W1S | 0h | Indicate if SOC20 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 19 | SOC19 | R-0/W1S | 0h | Indicate if SOC19 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 18 | SOC18 | R-0/W1S | 0h | Indicate if SOC18 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 17 | SOC17 | R-0/W1S | 0h | Indicate if SOC17 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 16 | SOC16 | R-0/W1S | 0h | Indicate if SOC16 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 15 | SOC15 | R-0/W1S | 0h | Indicate if SOC15 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 14 | SOC14 | R-0/W1S | 0h | Indicate if SOC14 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 13 | SOC13 | R-0/W1S | 0h | Indicate if SOC13 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 12 | SOC12 | R-0/W1S | 0h | Indicate if SOC12 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 11 | SOC11 | R-0/W1S | 0h | Indicate if SOC11 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 10 | SOC10 | R-0/W1S | 0h | Indicate if SOC10 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 9 | SOC9 | R-0/W1S | 0h | Indicate if SOC9 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 8 | SOC8 | R-0/W1S | 0h | Indicate if SOC8 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 7 | SOC7 | R-0/W1S | 0h | Indicate if SOC7 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 6 | SOC6 | R-0/W1S | 0h | Indicate if SOC6 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 5 | SOC5 | R-0/W1S | 0h | Indicate if SOC5 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 4 | SOC4 | R-0/W1S | 0h | Indicate if SOC4 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 3 | SOC3 | R-0/W1S | 0h | Indicate if SOC3 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 2 | SOC2 | R-0/W1S | 0h | Indicate if SOC2 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 1 | SOC1 | R-0/W1S | 0h | Indicate if SOC1 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
| 0 | SOC0 | R-0/W1S | 0h | Indicate if SOC0 selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: SYSRSn |
ADCSOCFRCGBSEL is shown in Figure 24-281 and described in Table 24-265.
Return to the Summary Table.
ADC Global SOC Force Select
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 |
| RESERVED | |||||||
| R-0-0h | |||||||
| 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | ADCE | ADCD | ADCC | ADCB | ADCA | ||
| R-0-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | R/W-0h | ||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-5 | RESERVED | R-0 | 0h | Reserved |
| 4 | ADCE | R/W | 0h | Indicate if ADCE selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: XRSn |
| 3 | ADCD | R/W | 0h | Indicate if ADCD selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: XRSn |
| 2 | ADCC | R/W | 0h | Indicate if ADCC selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: XRSn |
| 1 | ADCB | R/W | 0h | Indicate if ADCB selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: XRSn |
| 0 | ADCA | R/W | 0h | Indicate if ADCA selected for global SW trigger 0 : Not selected for Global SW Trigger 1 : Selected for Global SW Trigger Reset type: XRSn |
PARITY_TEST_ALT1 is shown in Figure 24-282 and described in Table 24-266.
Return to the Summary Table.
Enables parity test
| 31 | 30 | 29 | 28 | 27 | 26 | 25 | 24 | 23 | 22 | 21 | 20 | 19 | 18 | 17 | 16 |
| RESERVED | |||||||||||||||
| R-0h | |||||||||||||||
| 15 | 14 | 13 | 12 | 11 | 10 | 9 | 8 | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
| RESERVED | TESTEN | ||||||||||||||
| R-0h | R/W-0h | ||||||||||||||
| Bit | Field | Type | Reset | Description |
|---|---|---|---|---|
| 31-4 | RESERVED | R | 0h | Reserved |
| 3-0 | TESTEN | R/W | 0h | 1010: Parity test feature is enabled All other values: Parity test feature is disabled Note: (1) When the parity test feature is enabled, actual registers are not accessible in the memory map. Instead, the parity values (final XOR output indicating the parity error) are accessible. Parity is computed for every byte and the corresponding parity error value is available at the bit-0 of every byte. Value of '1' written to the parity bit after enabling the parity test feature can be used to inject the error by inverting the stored parity value. (2) It is recommended to leave the field as 0101 or 0000 after completing the parity test. Reset type: SYSRSn |