SWRU455M February 2017 – October 2020 CC3120 , CC3120MOD , CC3130 , CC3135 , CC3135MOD , CC3220MOD , CC3220MODA , CC3220R , CC3220S , CC3220SF , CC3230S , CC3230SF , CC3235MODAS , CC3235MODASF , CC3235MODS , CC3235MODSF , CC3235S , CC3235SF
The SimpleLink Wi-Fi device Wi-Fi Direct settings are configured by using the host driver API which controls the device. Several configurations for each specific use case exist. Some of the configurations are persistent according to the system-persistent configuration, and some are nonpersistent, as specified in each configuration specification (more information is in Section B). Not all configurations must be manually set by the user because the device has default values according to Table 5-10, which lists the Wi-Fi Direct default parameters.
| Configuration | Default Value |
|---|---|
| Interface | IPv4 |
| STA Tx power | 0 (no backoff, maximum Tx power) |
| Country code | EU |
| Connection policy | Auto and Auto Provisioning |
| Calibration mode | Normal |
| Applications | HTTP server |
| Intent | 3 |
| Negotiator | 2 |
| CL address | DHCP |
| GO address | Static with the following parameters:
IP 10.123.45.1, Subnet mask: 255.255.255.0 Default gateway: 10.123.45.1, DNS: 10.123.45.1 |
| Device name | mysimplelink_XX (xx = Random 2 characters) |
| Device type | 1-0050F204-1 |
| listen channel | Random channel between 1, 6, or 11 |
| Operational channel | Random channel between 1, 6, or 11 |