SLAAEG4B October 2023 – July 2025 MSPM0C1104 , MSPM0C1105 , MSPM0C1106 , MSPM0H3216 , MSPM0L1306
In MSPM0C1105 and MSPM0C1106 which support COMP, the VBOOST circuit in the PMU generates an internal VBOOST supply that is used by the analog mux in COMP. The VBOOST circuit enables consistent analog mux performance across the external supply voltage (VDD) range.
In MSPM0C1105 and MSPM0C1106, SYSCTL automatically manages the enable request for the VBOOST circuit based on the following parameters:
VBOOST is disabled by default following a SYSRST. Use the application software to enable the VBOOST circuit before using the COMP. When a COMP is enabled by application software, SYSCTL also enables the VBOOST circuit to support the analog peripheral.
The VBOOST circuit has a startup time requirement (12µs typical) to transition from a disabled state to an enabled state. In the event that the startup time of the COMP is less than the VBOOST startup time, the peripheral startup time is extended to account for the VBOOST startup time.
The PMU provides a temperature and supply voltage stable bandgap voltage reference which is used by the device for internal functions, including:
The bandgap reference is enabled in RUN, SLEEP, and STOP modes. Bandgap voltage operates in a sampled mode in STANDBY to reduce power consumption, and is disabled in SHUTDOWN mode. SYSCTL manages the bandgap state automatically, no user configuration is required.