SLAAEG4B October 2023 – July 2025 MSPM0C1104 , MSPM0C1105 , MSPM0C1106 , MSPM0H3216 , MSPM0L1306
To reduce the reflections on high speed signals, match the impedance between the source, sink and transmission lines. The impedance of a signal trace depends on the geometry and the position with respect to any reference planes.
The trace width and spacing between differential pairs for a specific impedance requirement is dependent on the chosen PCB stack-up. As there are limitations in the minimum trace width and spacing which depend on the type of PCB technology and cost requirements, a PCB stack-up needs to be chosen which allows all the required impedances to be realized.
The minimum configuration that can be used is 2 stack-up. A 4- or 6-layer boards is required for very dense PCBs that have multiple high-speed signals.
The following stack-up (see Figure 9-5) is a 4-layer examples that can be used as a starting point for helping in a stack-up evaluation and selection. These stack-up configurations are using a GND plane adjacent to the power plane to increase the capacitance and reduce the gap between GND and power plane. High speed signals on the top layer can have a solid GND reference plane, which help to reduce EMC emissions, as going up in number of layers and having a GND reference for each PCB signal layer further improves the radiated EMC performance.
Figure 9-5 Four-Layer PCB Stack-up
ExampleIf the system is not very complicated, then there is no high-speed signal or some sensitive analog signal, then the 2 stack-up structure is sufficient.