SLUUDM5 March 2026 MSPM0G1507 , MSPM0G1519 , MSPM0G3507 , MSPM0G3519
Set mtrStartUpOption as 3h to select slow first cycle mode. In slow first cycle start-up, the FOC algorithm starts motor commutation at a frequency defined by pUserInputRegs->mtrStartUp2.b.slowFirstCycFreq. The frequency configured is used only for first cycle, and then the motor commutation follows acceleration profile configured by open loop parameters, as shown in the following figure. The slow first cycle frequency has to be configured to be slow enough to allow motor to synchronize with the commutation sequence. This mode is useful when fast startup is desired as it significantly reduces the align time.
Set pUserCtrlRegs->algoDebugCrtl1.b.forceSlowCycleFirstCycleEn to 1b to enable force slow first cycle mode for debug usage.