SLUUDM5 March 2026 MSPM0G1507 , MSPM0G1519 , MSPM0G3507 , MSPM0G3519
FOC application uses a pre-defined symbol to determine which gate driver board is used to configure the board parameters and HAL layer properly, as shown in the following figure.
The default gate driver interface is configured for the EVM hardware board. Users can overwrite the relevant configuration set for DRV8316 to their own board configuration.
While recommend using CUSTOM symbol for users’ specific hardware design if use another gate driver for better code management. Follow the steps below to configure the Custom Gate Driver Module with this approach.