SLUUDM5 March 2026 MSPM0G1507 , MSPM0G1519 , MSPM0G3507 , MSPM0G3519
In power control mode, the input electrical power of the motor (Watts) is controlled using a closed loop PI control according to the input reference set as speedInput value in Speed Control Register (P.U value in IQ15 format). The P.U power is computed as the ACTUAL_MOTOR_POWER / MAX_MOTOR_POWER value configured in systemParams.
Example: For maxMotorPower set to 100Watts, setting reference Input in speedInput to 0x3FFFh (0.5 P.U in IQ15) operates the Motor at a constant electrical power of 50W.
FOC algorithm uses power closed loop control by setting controlMode as 1h.