SLUUDM5 March 2026 MSPM0G1507 , MSPM0G1519 , MSPM0G3507 , MSPM0G3519
The FOC structure for a PMSM is illustrated in Figure 2-2. In this system, the eSMO is used for achieving the sensorless control an IPMSM system, and the eSMO model is designed by utilizing the back EMF model together with a PLL model for estimating the rotor position and speed.
An IPMSM consists of a three-phase stator winding (a, b, c axes), and permanent magnets (PM) rotor for excitation. The motor is controlled by a standard three-phase inverter. An IPMSM can be modeled by using phase a-b-c quantities. Through proper coordinate transformations, the dynamic PMSM models in the d-q rotor reference frame and the α-β stationary reference frame can be obtained. The relationship among these reference frames are illustrated in the following equation. The dynamic model of a generic PMSM can be written in the d-q rotor reference frame as:
Where vd and vq are the q-axis and d-axis stator terminal voltages, respectively; id and iq are the d-axis and q-axis stator currents, respectively; Ld and Lq are the q-axis and d-axis inductances, respectively, p is the derivative operator, a short notation of ; λpm is the flux linkage generated by the permanent magnets, Rs is the resistance of the stator windings; and ωe is the electrical angular velocity of the rotor.
By using the inverse Park transformation as shown above, the dynamics of the PMSM can be modeled in the α-β stationary reference frame as:
Where the ea and eβ are components of extended electromotive force (EEMF) in the α-β axis and can be defined as:
According to these equations, the rotor position information can be decoupled from the inductance matrix by means of the equivalent transformation and the introduction of the EEMF concept, so that the EEMF is the only term that contains the rotor pole position information. And then the EEMF phase information can be directly used to realize the rotor position observation. Rewrite the IPMSM voltage equation below as a state equation using the stator current as a state variable:
Since the stator current is the only physical quantity that can be directly measured, the sliding surface is selected on the stator current path:
where and are the estimated currents, the superscript (^ ) indicates the estimated value, the superscript (~) indicates the variable error which refers to the difference between the observed value and the actual measurement value.