If the EVM does not work as expected, consider the
following:
Verify hardware setup:
- Do not make modifications to the
EVM or change the default settings until AFTER the EVM is verified to be
working.
- Validate power supply is connected, is turned on, and current limit is
appropriate for the device.
- Validate OSCIN signal is supplied, is turned on with appropriate output
level.
- Verify that the spectrum analyzer
center frequency matches target frequency. Choose wide span so that the carrier
can be seen if the frequency is off from center.
- Verify that the device is not
powered down by the CAL pin in Pin Mode.
- When the EVM is in Pin Mode,
- Power up current of the EVM is approximately 240mA if CAL header is
strapped.
- Power up current of the EVM is approximately 16mA if CAL header is open.
- When the EVM is connected to a PC,
- Power up current of the EVM is approximately 240mA if TICS Pro with EVM
Default Mode configuration is loaded.
- Power up current of the EVM is approximately 16mA, otherwise.
- For LMX2624SPEVM and
LMX2695SEPEVM,
- If onboard LDO is used, there is an additional 20mA current drawn due to
the LDO.
- If onboard LDO is used,
both VBIAS and VCCIN supplies are required.
Verify software setup:
- If your configuration is not
working, revert back to EVM Default Mode configuration, validate the device is
locked and then modify the device again to your configuration.
- Validate that no red warning is prompted. If so, mouse over to the warning
element, read the tool tips or check the message in the bottom left status
window.
- Click the Reset device button once to reset the device, then load
all the registers.
- With No Assist operation, after changing the VCO frequency or enabling VCO
doubler output, a VCO calibration is required. Click the Calibrate
VCO button to initiate VCO calibration.
- Register read back requires the correct configuration, see Figure 4-18 for details.
Verify PC communications:
- In the menu bar, click USB
Communications → Interface. Verify that the USB2ANY button is
turned green. Click Identify to validate the USB LED on the EVM
blinks.
- Program POWERDOWN = 1 to validate there is significant current
change.