SNAU308A November 2024 – May 2025
The SYNC pulse being used for Category 3 synchronization requires a certain setup and hold time with respect to the input reference clock. This requirement is to verify that all the devices use the same input clock edge to start synchronization. MASH_RST_COUNT must be set to provide sufficient time for the synchronization to complete.
Figure 4-35 Category 3 SYNC
ConfigurationIf a non time-critical SYNC pulse is used for Category 3 SYNC, or after a VCO calibration, the phase between devices is not identical.
Figure 4-36 Not Synchronous Example
1
Figure 4-37 Not Synchronous Example
2With a time-critical SYNC pulse, the output phase is aligned. Please note that the output phase of each device can not be exactly the same, but the difference remain unchanged after synchronization.
Figure 4-38 Time Critical SYNC
Pulse
Figure 4-39 Category 3 SYNC