SNAU308A November 2024 – May 2025
The MASH_SEED word can use the sigma-delta modulator of the PLL to shift output signal phase with respect to the input reference clock. To enable phase adjustment, set MASH_SEED_EN = 1 and then program a value to MASH_SEED. Alternatively, a desired phase shift value can be used with TICS Pro calculating the MASH_SEED value. There are some restrictions in using phase adjustment, click the Help button to see the details.
Figure 4-31 Phase Adjustment
Configuration
Figure 4-32 Phase Adjustment