SNAU308A November 2024 – May 2025
Every time the VCO frequency is changed, instead of performing a VCO calibration, Full Assist operation specifies the VCO core and band for the PLL to lock. As a result, there is no VCO calibration time involved. The total time taken to switch VCO frequency is equal to register programming time plus PLL lock time.
To be able to know which VCO core and band to use for a specific VCO frequency, a one-time VCO calibration needs to be performed, a register read back needs to be performed to collect this information, and the information needs to be stored in a look up table (LUT). In addition to the VCO parameters, if VCO doubler is used, VCO doubler parameters can be obtained in the similar fashion. For example, again switching the VCO frequency between 7500MHz and 15GHz. RFOUTA is divide by 4 output. With Full Assist operation, the lock time (excluding register programming time) is less than 20µs.
Figure 4-16 Full Assist Jump
Down
Figure 4-17 Full Assist Jump
UpA. LUT creation
Figure 4-18 LUT Creation
Figure 4-19 Full Assist
ProgrammingB. Apply LUT data